2011-12-27 5:30 PM
Hi, first of all sorry for my english but I hope you will understand me.
Here is a TIM1 configuration form DSO nano project. I've rewrited it to more readable format:TIM1->PSC = 30;TIM1->ARR = 35;TIM1->CCR1 = (35+1)/2;TIM1->CR1 = TIM_CR1_DIR | TIM_CR1_URS | TIM_CR1_ARPE;TIM1->RCR = 0x0000;TIM1->CCER = TIM_CCER_CC1E;TIM1->CCMR1 = TIM_CCMR1_OC1FE | TIM_CCMR1_OC1PE | TIM_CCMR1_OC1M;TIM1->BDTR = TIM_BDTR_MOE;TIM1->DIER = TIM_DIER_CC1DE |TIM_DIER_UDE | TIM_DIER_TDE;TIM1->CR1 = TIM_CR1_CEN;Can somebody explain me how this configuration behave? Am I correct if I think the period of occuring events is (PSC+1)*(ACC+1)/72MHz ? (does the TIM1->CCR1 = (35+1)/2; have any meaning?) How works bits TDE and UDE?I take a simple experiment with this configuration with set bits TDE UDE and without them but I dont see any difference (of course in DMA usage).2011-12-28 9:16 AM
Pretty limited desire to decipher bit level TIM configurations.
The value of ARR suggests a frequency of about 64.516 KHz. The computation for CCR1 suggests a desire for a 50/50 duty cycle.2011-12-28 9:52 AM
Thank You for reply. This configuration in general was created to trigger ADC by timer's events. Does the duty cycle (in this case 50%) have any effect to the frequency of events? What would be in case of ex. 10% duty cycle?
What do CC1DE, UDE and TDE bits dopractically
?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.