2021-03-22 1:15 AM
The TCP network of NETX generated by CubeMX does not run successfully.I have studied ST's NETXduo example and tried many possibilities, but it still doesn't work. The development board is NUCLEO-H743ZI.
2022-12-12 2:51 AM
Hi,
Looking into your .ioc file I see some configurations which can cause problems such as :
Also in the .sct file, there's a missing definition sections.
I suggest you to align your project with the last STM32Cube MCU Package for STM32H7 (V1.11.0) available here.
Then, concerning app configuration, refer to :
Please, update your project, and if the problem persist, do not hesitate to share it.
Regards
Mahdy
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.