2018-06-12 7:58 AM
2018-06-13 12:01 AM
Because it has a fixed value ?
https://www.tai-tech.com.tw/_upload/files/FCM1608-Series.pdf
Some while ago, I would perhaps have said 'Google Is Your Friend'. Not so sure anymore ...
2018-06-13 2:46 AM
,
,
But not even in the attached document is the inductance mentioned, I have
searched everywhere but I have not found it.
2018-06-13 9:03 GMT+02:00 AvaTar <,st-microelectronics@jiveon.com>,:
STMicroelectronics Community
<,https://community.st.com/?et=watches.email.thread>,
Re: The STM32F407G-DISC1 board L1 'fcm1608-0603' inductor
reply from AvaTar
<,
in STM32 MCUs Forum - View the full discussion
<,https://community.st.com/0D70X000006SqPhSAK
2018-06-13 8:49 AM
That component is not used as an inductor. It's a ferrite bead and meant to suppress certain frequencies. If you don't care about passing EMC tests you can use a short instead.
2018-06-14 1:51 AM
Ok, understood. By the way, in the document several are rated for different
DC resistance and MAX current. The one on the board will be a medium one
according to the current consumed by the uC?
2018-06-13 15:50 GMT+02:00 mich.lei <st-microelectronics@jiveon.com>:
STMicroelectronics Community
<https://community.st.com/?et=watches.email.thread>
Re: The STM32F407G-DISC1 board L1 'fcm1608-0603' inductor
reply from mich.lei
<
MCUs Forum* - View the full discussion
<https://community.st.com/0D70X000006Sy5GSAS
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.