2018-08-08 8:56 AM
The *.stldr file generated by MX25LM51245G_STM32L4R9I-DISCO (@ ST-LINK Utility 4.2.0.0) can't work for STM32L4R9I-DISCO device.
Step1. According to the readme.txt in the directory of "C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader\MX25LM51245G_STM32L4R9I-DISCO", The detail is as follows:
@par Example Description
This an example of an external loader of MX25LM51245G flash memory for STM32L4R9I-DISCO.
This loader can be used with STM32 ST-LINK Utility and STM32CubeProgrammer.
@par Hardware and Software environment
- This example runs on STM32L4R9xx devices.
- This example has been tested with STMicroelectronics STM32L4R9I-Discovery
boards and can be easily tailored to any other supported device
and development board.
@par How to use it ?
- Place the folder "MX25LM51245G_STM32L4R9I-DISCO" under the following path inside the STM32L4 Cube firmware package "STM32Cube_FW_L4_Vx.y.z" folder:
STM32Cube_FW_L4_Vx.y.z\Projects\STM32L4R9I_DISCO\Examples\OSPI
- Open your preferred toolchain
- Rebuild all files and load your image into target memory
- After build, the loader should be displayed in the external loaders window, ready-to-use.
Step2. Add Existing project of MX25LM51245G_STM32L4R9I-DISCO by using the EWARM 8.22.1,then rebuild all files.So the
*.out file will be generated, then rename to *.stldr and copy to the directory of "C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader\"
IAR Configuration
Step3. When downloading MenuLauncher-STM32L4R9I-Discovery_V1.0.0.hex through ST-Link Utility 4.2.0.0,the error is as following:
23:49:29 : ST-LINK SN : 0678FF504955857567011028
23:49:29 : ST-LINK Firmware version : V2J29M18
23:49:29 : Connected via SWD.
23:49:29 : SWD Frequency = 4,0 MHz.
23:49:29 : Connection mode : Connect Under Reset.
23:49:29 : Debug in Low Power mode enabled.
23:49:29 : Device ID:0x470
23:49:29 : Device flash Size : 2MBytes
23:49:29 : Device family :STM32L4Rx
23:50:24 : [MenuLauncher-STM32L4R9I-Discovery_V1.0.0.hex] opened successfully.
Address Ranges [0x08000000 0x080001BC] [0x08006000 0x08006F48] [0x08007000 0x0803B303] [0x90000000 0x9022C30A]
23:50:24 : [MenuLauncher-STM32L4R9I-Discovery_V1.0.0.hex] checksum : 0x0F9EA60A
23:52:26 : Timeout during flash programming
23:52:26 : Error occured during erase operation!
Best Regards,
2018-12-01 4:23 AM
For starting, I just want to be able to compile an external loader for the STM32L4R9 Discovery Board by my own. I can compile but that elf does not work with the ST-Link programmer. For the posts here, I guess that the example project has some issue. So could you share the project for the Discovery? Thanks.
2019-01-03 9:18 AM
-Please find attached the corrected project it works well on the STM32L4R9 discovery and STLink utility 4.2.0.
Please find a nice step-by step powerpoint that explains how to configure
the QSPI Flash interface from CubeMx and the memory data sheet, how To test it (and optimize) and
how add the STLIink loader C files and atollic linker file to make a loader application (.stldr).
The idea is to provide a universal method whatever the board pinout and memory to configure the qspi then create your own external flash loader.
Br
Emmanuel Combette
STMicroelectronics Tomas team
2019-01-03 9:27 AM
Project source code.
On discovey the flash is connected to OctSPI_SPI2 interface starting on 0x7000 0000.
The descriptor in the flash loader starts Def_inf.c is incorrect , the start address is the OctoSPI_SPI1 interface and the comments are not aligned with the L4R9 memory map and data sheet.
2019-01-03 9:29 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.