2018-10-22 2:54 PM
Hi ST community members,
I have SMT32 card and pulse sensor that allows to measure the heart beat (ECG signal). In fact, I want to visualize the samples of ECG signal at the output of ADC through matlab. More precisely, I want to present the samples with amplitudes (not binary i.e; just the sampling phase without quantization) in real time with matlab.
So, I wonder if there is a solution of interconnction of stm32 and matlab in this way becasue I found only the interconnection via similink!!
Thanks in advance!!
2022-05-30 2:23 AM
Hello,
I already the exercise using Octave. I would recommend you to use the serial com port interface to get/read your desired data.
Your script could query/read regularly your samples and plot it using a graphical interface under matlab/octave.
Here an octave existing example : https://lists.gnu.org/archive/html/help-octave/2016-05/msg00197.html
Regards,
Simon
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.