cancel
Showing results for 
Search instead for 
Did you mean: 

The µC STM32F051Kx has only one SPI and of course only one CS (chip select). It is possiblie to use another and configure it as CS?

SAbis
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Uwe Bonnes
Chief

Of course you can bitbang other pins as CS.

thanks very much.

do you have any idea on using the UART interface to upload Firmware? We are using only this interface to communicate between our controller and to reduce the Pin-number and an extra connector for SWD (serial wired debu), I am planning directly to use the same communication interface (RS485) to upload my firmware. is this possible? if yes how could i realise it in Hardware?

Thanks

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.