2021-01-06 2:30 PM
So I have a NUCLEO-G070RB board here and I am not using the HAL library, but just CMSIS libraries.
I see the SysTick functions are part of the HAL not CMSIS. is there a particular reason? I would figure since it's part of the M0+ core it would be in CMSIS.
Unless I missed something somewhere...
ARM in new to me so go easy;)
Thanks
2021-01-06 2:44 PM
>>Is there a particular reason?
Who knows, is it worth pondering, or can you just cut-n-paste the things you need and move forward?
2021-01-06 4:19 PM
What is "CMSIS libraries"?
JW
2021-01-06 4:34 PM
Except for ISR itself, I can see only one SysTick function and it is a part of CMSIS:
https://www.keil.com/pack/doc/CMSIS/Core/html/group__SysTick__gr.html
And to be completely fair... System ticks as a part of a driver library is a bad idea. If any library needs such a functionality, it should use the system/OS/platform provided one. But there is the catch - Cube/HAL team is not even capable of analyzing and deciding what HAL is and what it isn't. Is it a low-level driver library or high-level platform API? Should it be thread-safe or not? In reality it's a bloatware of something from everything tossed together by careless beginners...
2021-01-07 8:22 AM
I found the defines in 'core_cm0.h'.
Thanks
2021-01-07 8:22 AM
Your right, It's not a Library but just header files. 'CMSIS Cortex-M0 Core Peripheral Access Layer Header File'
Thanks
2021-01-07 8:22 AM
This is what I was looking for. But I had over looked it somehow.
Not looking to reinvent the wheel here.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.