2021-11-17 4:13 PM
My goal is to start ADC conversions a deterministic amount of time after raising a GPIO.
Since the ADC clock is slower than the instruction clock, the instruction to set SWSTART can occur in between ADC clock cycles. I currently have the ADC clock set to fPCLK2/2 and PCLK to HCLK/2, so I see up to 3 instruction cycles of jitter between raising the GPIO and starting the samples. Is there a technique useful for eliminating this jitter?
2021-11-18 5:52 AM
One possibility would be to use a timer to trigger the ADC and use the same timer to generate the GPIO edge. If the timer runs at the ADC speed, it should be consistent.
2021-11-18 8:45 AM
Thank you for your reply. I will investigate this option.
I will need to use the interrupt for the timer? Just checking flags introduces jitter. Unfortunately the hardware I have inherited does not use a pin that is attached to a timer. The ISR needs to be in ITCM as well?
2021-11-18 9:09 AM
2021-11-18 9:47 AM
> Unfortunately the hardware I have inherited does not use a pin that is attached to a timer.
Namely?
JW
2021-11-18 10:28 AM
The GPIO pin on the hardware I inherited is not connected to a timer, however. It seems the best I can do is use an interrupt, raise the pin with an instruction, and then start the adc deterministically wrt the timer that caused the interrupt?
2021-11-18 10:29 AM
The hardware was designed by a contractor who I have replaced. The company owns a lot of these boards, however, and I need to do the best I can with what I have.
2021-11-18 1:12 PM
No, I mean, which pin exactly is the one you want to output the sync onto.
JW
2021-11-19 6:12 AM
There are several pins. PB0-2, PE2-4, and PE9-PE14.
2021-11-19 6:25 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.