2013-12-10 2:15 AM
Hi,
I've been using MikroElektronika as my IDE for the last couple of months but am now at the stage where I'm growing very frustrated with it's bugs and issues. Was wondering what others are using and what you would recommend? Cheers!2013-12-13 11:34 AM
I'm a begginer.
After trying some six IDE's, i've settled for Atollic Truestudio light. The examples that come with Discovery board compile and work out of the box (only one exceeded 32k code size limit), and there are lots of projects online using Atollic. Still, in the future, for bigger projectes (RTOS etc.), one should get used to open source tools, I guess...2013-12-15 8:35 PM
For the past weeks I have used several of the free IDE alternatives. My conclusion is that the
Em::Blocks
(http://www.emblocks.org) is the best. The ST firmware for STM32F401/F429 supports directly only EWARM, MDK-ARM, and TrueSTUDIO. With the cooperation on the EmBlocks site, I did create the missing project files to enable immediate development of your own applications using the ST firmware for these two excellent boards. Please feel free to contact me for the project files.2013-12-19 1:23 AM
Thanks Ollie, will give it a try.
2014-01-05 9:12 AM
Have you been able to get the StlinkGDB to run? I keep getting errors that it can't find my device.
2014-01-05 7:12 PM
The debugger has been a challenge for me. Everything was OK with emBlocks 1.40. After upgrading to 1.41 and 1.42 I have not been able to use the debugger with emBlocks. My F401 and F429 debugging still works with IAR EW - thus the problem is not in H/W or core S/W. I am waiting resolution from emBlocks developer.
I have left the default GDB server selection (STLinkGDB.exe 1/1/14 version)) in Debugger Interface Options. When starting the download (F8), the command line window flashes and then the error dialog window opens.2014-01-05 7:30 PM
That's the same thing that's happening to me. I've even tried launching from the command line. It must be a bug in the latest windows builds of STLink (the open source version).
2014-01-06 7:23 AM
With the help of the emBlocks developer, the problem is now solved.
The other STLinkGDB clients have the proper support for USB3. With emBlocks you have to use USB2 or special USB drivers. In my case, I had the USB3 in my Dell monitor and I didn't realize that. In my computer all USB3 connectors are blue and USB2 connectors are black. Once I connected STM32F4xx to my Dell keyboard (USB2) things resumed to work OK. I did install the USB3 Renesas driver (http://downloadmirror.intel.com/19880/eng/USB3.0_allOS_2.1.28.1_PV.exe). After that, I can connect STM32F4xx to the USB3 port in my computer. This is not solving the USB3 problem in Dell monitor.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.