2011-04-14 5:33 AM
STOP mode and BOOT0 pin
2011-05-17 5:31 AM
I agree that beyond specifying BOOT0 as an INPUT, there's no other technical information. I would guess that the pin is a genuine floating input without pull up or pull down as these are associated with Input / Output pins. Also, where ST have used integrated resistors as on the JTAG pins they have documented it.
Why not submit a Technical Support query and report back the answer here?2011-05-17 5:31 AM
It's floating input.
We have it pulled to ground, and in STOP mode we consume around 30uA.2011-05-17 5:31 AM
Hi Domen,
thank you for your response.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.