2024-08-29 10:19 AM
libusb: info [darwin_claim_interface] no interface found; setting configuration: 1
Device : MACBOOK AIR
STMicroelectronics ST-LINK GDB server. Version 7.5.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
libusb: error [darwin_claim_interface] could not set configuration
Device connect error
Error in initializing ST-LINK device.
Reason: Failed to connect to device. Please check power and cabling to target.
2024-08-29 5:28 PM
Try to connect the ST-LINK thru a hub (better a powered one).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.