2013-11-15 11:18 AM
Dear friends,
I'll be using stm32f4 discovery with Matlab embedded coder. Now I'm not quite sure if this is the right place to ask for Matlab help,but my queries are solely related to the hardware programming.Now my objective is simple. I want my board adc to trigger when some external high to low pulse occurs on a gpio pin. Only thing I want to do this task on simulink. I could initialise the ADCs GPIOs, but the connection for the external trigger seems to be tricky. Yes I'm not much conversant with the embedded coder, looking forward for some help in this regard.Thanks & regards,Souvik2013-11-25 5:10 AM
2013-11-25 11:57 PM
Thanks a lot
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.