2015-12-22 1:47 AM
Hello!
I have already coded for CAN Loopback mode and it works.
However, when I changed the mode to CAN Normal Mode, I am unable to hit Receive Handler, but I can hit transmit Handler.int main(void)
{/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();/* Configure the system clock */
SystemClock_Config();/* Initialize all configured peripherals */
MX_GPIO_Init(); MX_CAN_Init();CanTxMsgTypeDef TxMsg = {
.StdId = 0x321, .ExtId = 0x01, .IDE = CAN_ID_STD, .RTR = CAN_RTR_DATA, .DLC = 1, }; CanRxMsgTypeDef RxMsg;hcan.pTxMsg = &TxMsg;
hcan.pRxMsg = &RxMsg; CAN_FilterConfTypeDef CAN_FilterConfig = { .BankNumber = 0, .FilterActivation = ENABLE, .FilterScale = CAN_FILTERSCALE_16BIT, .FilterMode = CAN_FILTERMODE_IDMASK, .FilterNumber = 0, .FilterFIFOAssignment = 0, .FilterMaskIdLow = (0x7FF << 5), .FilterMaskIdHigh = (0x400 << 5), .FilterIdLow = (CAN_ID << 5), .FilterIdHigh = (2047 << 5), }; HAL_CAN_ConfigFilter(&hcan, &CAN_FilterConfig);HAL_CAN_Receive_IT(&hcan, CAN_FIFO0);
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_9, GPIO_PIN_RESET); //CAN initialisation over hcan.pTxMsg->Data[0]++; HAL_CAN_Transmit_IT(&hcan); //transmit interrupt hits after this HAL_Delay(10); uint32_t i = 0; while((i < 0xFFF)) { i++; }while (1)
{ }}
void USB_LP_CAN_RX0_IRQHandler(void)
{HAL_GPIO_WritePin(GPIOC, GPIO_PIN_9, GPIO_PIN_RESET);
HAL_CAN_IRQHandler(&hcan);}
void USB_HP_CAN_TX_IRQHandler(void)
{ HAL_GPIO_WritePin(GPIOC, GPIO_PIN_9, GPIO_PIN_RESET); HAL_CAN_IRQHandler(&hcan); }void HAL_CAN_TxCpltCallback(CAN_HandleTypeDef* hcan)
{ uint32_t timeout = 500; HAL_StatusTypeDef status;status = HAL_CAN_Receive_IT(hcan, CAN_FIFO0);
if(HAL_OK != status){ while(1); } }I have also put the following in HAL_CAN_MspInit function:
HAL_NVIC_SetPriority(USB_LP_CAN_RX0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USB_LP_CAN_RX0_IRQn); HAL_NVIC_SetPriority(USB_HP_CAN_TX_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USB_HP_CAN_TX_IRQn);Is it a sequencing issue? I am not sure why receive handler is not getting it (i.e. USB_LP_CAN_RX0_IRQHandler cannot be hit). Please help! Any help is appreciated! Thank you!
#can #stmf303 #can-normal-mode2015-12-22 10:03 AM
Check the CAN error status register and if no errors then your RX filters to determine why you cannot receive. Are both nodes showing the same problem (you need a minimum of two CAN nodes to send and receive)?
Jack PeacockWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.