2024-03-28 9:35 AM
I am unable to switch on the AUTOFF bit in ADC4.
DS reads about ADC_PWRR/AUTOFF: The software is allowed to write this bit only when ADEN bit is cleared to 0 (this ensures that no conversion is ongoing).
But if this bit is set, the ADC doesn't set ADRDY flag if enabled.
LL_ADC_SetLPModeAutoPowerOff(ADC4, LL_ADC_LP_AUTOPOWEROFF_ENABLE);
LL_ADC_ClearFlag_ADRDY(ADC4);
LL_ADC_Enable(ADC4);
while(!LL_ADC_IsActiveFlag_ADRDY(ADC4)) {} // here waits forever
If I omit the ADRDY check and simply wait some time and then I start the conversion, the ADC works and converts inputs correctly.
If I omit the AUTOFF setting, the code works ok. If I try to set the bit after enable, the bit remain unchanged (acording to DS)..
My question is: How to set the AUTOFF bit? Isn't it a bug in silicon?
2024-05-02 8:47 AM
Hi @Tomas Hamouz,
Coming back to your question, I hope it was solved since the time you asked it. That would be interesting to share your findings.
On my side, I have following 2 proposals:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.