2022-01-27 5:17 PM
In STM32U575/585 RM0456 Rev 2 from September 2021, I see the following:
"11.4.7 LSE clock
...
External source (LSE bypass)
In this mode, an external clock source must be provided. It can have a frequency of up to 1 MHz."
However, in STM32U585xx DS13086 Rev 4 from December 2021, I see the following:
"5.3.7 External clock timing characteristics
...
Table 78. Low-speed external user clock characteristics
f_LSE_ext - User external clock source frequency
Min: 5 kHz
Typ: 32.768 kHz
Max: 40 kHz"
So, is the max LSE frequency in bypass mode 1 MHz or is it 40 kHz? On previous MCU families such as the STM32G4 an LSE frequency up to 1 MHz in bypass mode was supported.
Thanks!
Solved! Go to Solution.
2022-01-28 1:38 AM
Hello @Terry Greeniaus
Thanks for reporting, it will fixed in next release of the RM (no more max LSE freq in it).
The reference is the current datasheet, so max freq 40kHz (even if it is was more in other MCU families)
BR,
Bruno
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-01-28 1:38 AM
Hello @Terry Greeniaus
Thanks for reporting, it will fixed in next release of the RM (no more max LSE freq in it).
The reference is the current datasheet, so max freq 40kHz (even if it is was more in other MCU families)
BR,
Bruno
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-01-28 1:45 AM
Thanks for your reply!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.