2025-08-18 12:30 AM
i DEBUG STM32N5670-DK Template_XIP_FSBL with stm32cubeide1.19.0 and ERROR comes:Device debug script
the detail is:
STMicroelectronics ST-LINK GDB server. Version 7.11.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61922
Status Refresh Delay : 15s
Verbose Mode : Disabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------
Log output file: C:\Users\supcon\AppData\Local\Temp\STM32CubeProgrammer_a04640.log
ST-LINK SN : 0038002E3333511*********
ST-LINK FW : V3J16M9
Board : STM32N6570-DK
Voltage : 3.27V
JTAG freq : 21333 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x486
Revision ID : Rev B
Device name : ST32N657
Device type : MCU
Device CPU : Cortex-M55
BL Version : --
Error: Erase command for internal Flash memory is not available for N6 devices.
Encountered Error when opening E:\ST\STM32CubeIDE_1.19.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.200.202503041107\tools\bin\STM32_Programmer_CLI.exe
Shutting down...
Exit.
i noticed that N6 has no internal FLASH?maybe?from:Nucleo N6 won't flash - STMicroelectronics Community
so,this is the reason why i cant debug N6?HOW can i fix it.
2025-08-18 7:51 AM
Hello @yipeng
The STM32N6 does not have internal Flash memory; instead, it features 128 KB of Boot ROM and 4.5 MB of RAM, with the option to expand memory externally.
The device boots from the Boot ROM and then either jumps to execute code directly from external Flash or copies the code into RAM for execution.
Regarding STM32CubeProgrammer, please try performing an ST-LINK firmware update.
You can refer to Application Note AN6265 , which explains how to debug an example using STM32CubeIDE.
Additionally, you can consult the Readme file of the project https://github.com/STMicroelectronics/STM32Cube
Kind regards,
2025-08-20 7:17 PM
thanks for your comment.
i conformed that the FSBL of tamplete Template_XIP_FSBL should be bebuged through RAM ONLY.
To simplify debug process,i turned it to TAMPLATE ,which is the most simplest template.
i open stm32n657xx_axisram2_fsbl.sct file which is for KEIL and noticed that LR_IROM1 is 0x34180400 and RW_IRAM1 is 0x341C0000 which verify that TAMPLATE should be bebuged through RAM.i change some settings in KEIL for debug - through-RAM and it works!i can debug , the LEDs flashing.
But,i failed to debug - through-RAM by STM32CUBEIDE,i changed lots of settings in “debug configuration” - “debuger” and “debug configuration” - “startup”,it didnt works.i view AN6265 and UM2609,but they do not mention debug - through-RAM configurations.is there more settings to setup a debug - through-RAM configuration?
thanks again!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.