2020-06-23 4:15 PM
I'm trying to use 3 GPIO Pins as a 3-bit ID essentially. Depending on the values read, the uC will configure itself in an appropriate way (1 bin fits all tools essentially). The problem I'm having is that with the eval board the pins are pretty close together, so I can only fit my jumper wires on the top corner pins of each section, vastly limiting the number i can test with.
I can get 2 pins that consistently behave correctly when I have the inputs driven/not driven, but the 3rd is always on a pin that constantly be in a HIGH state even at initialization. How do I fix this?
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
Configure_Card_GPIO_Init();
Configure_Card_Type(gpioSelection);
....
}
static void Configure_Card_Type(int gpio_lines)
{
uint8_t cal_value = 0;
cal_value += HAL_GPIO_ReadPin(GPIO_CAL_E13_GPIO_Port, GPIO_CAL_E13_Pin);
cal_value = cal_value << 1;
cal_value += HAL_GPIO_ReadPin(GPIO_CAL_F11_GPIO_Port, GPIO_CAL_F11_Pin);
cal_value = cal_value << 1;
cal_value += HAL_GPIO_ReadPin(GPIO_CAL_E0_GPIO_Port, GPIO_CAL_E0_Pin);
.... do things
}
static void Configure_Card_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOF_CLK_ENABLE();
/*Configure GPIO pins : GPIO_CAL_E1_Pin GPIO_CAL_E2_Pin GPIO_CAL_E0_Pin */
GPIO_InitStruct.Pin = GPIO_CAL_E13_Pin|GPIO_CAL_E14_Pin|GPIO_CAL_E0_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/*Configure GPIO pin : GPIO_CAL_F11_Pin */
GPIO_InitStruct.Pin = GPIO_CAL_F11_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(GPIO_CAL_F11_GPIO_Port, &GPIO_InitStruct);
}
Solved! Go to Solution.
2020-06-23 6:42 PM
Double check that the pin is not connected to anything else. There is no reason it shouldn't behave the same as the other pins. There has to be a reason either in the code, the board, or possibly due to damage. Nothing special about any of the pins you're trying that I can think of.
Set the pin as GPIO and see if you can toggle it high and low.
2020-06-23 6:42 PM
Double check that the pin is not connected to anything else. There is no reason it shouldn't behave the same as the other pins. There has to be a reason either in the code, the board, or possibly due to damage. Nothing special about any of the pins you're trying that I can think of.
Set the pin as GPIO and see if you can toggle it high and low.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.