2024-04-16 6:13 AM
Hi There,
I'm trying to set the clock configuration of an STM32L4S5 and have spotted some ambiguities in the reference manual concerning the maximum input frequency to the PLL:
RM0432 6.4.4 says the following in the context of choosing the M value when programming the PLL:
The software has to set these bits correctly to ensure that the VCO input
frequency ranges from 2.66 MHz to 8 MHz
RM0432 6.2.5 says the following:
The PLLs input frequency must be between 4 and 16 MHz. The selected clock source is divided by a programmable factor PLLM from 1 to 8 to provide a clock frequency in the requested input range
DS12024 6.3.9 Gives a range of 2.66 - 16 MHz for FPLL_IN.
My configuration runs the MSI at 48 MHz, feeds this into the M divider for a 16 MHz output to the PLL, which provides an output of 80 MHz. Is this a valid configuration? Should I instead be increasing M to reduce the PLL input to 8 MHz?
Thanks in advance!
Kevin
2024-04-16 6:26 AM
Hi,
to be in the middle of the allowed range is probably best ; (2.66 MHz to 8 MHz );
so i would set prescaler to 6 MHz for VCO input. (8 is also still ok.)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.