2016-01-24 11:27 PM
Hi,
I am using STM32L476 controller. When I am trying to initialize internal RTC with LSI clock using ST example code, it is returning timeout. When I debugged the code I observed it is inRTC_EnterInitMode() function and returning timeout at below condition.
/* Wait till RTC is in INIT state and if Time out is reached exit */
while((hrtc->Instance->ISR & RTC_ISR_INITF) == (uint32_t)RESET)
I have verified the LSI clock frequency it is 32K. Can someone please tell me what can be the problem? Thank you. Lucky #!stm32-!cubemx-!rtc-!timeout #!stm32We’re moving the ST Community to a new platform to give you a better and more reliable community experience.