2018-12-26 4:10 PM
please somebody help me.
i really need the STMAP File supports STM32L433CCUX. i cannot see this stmap file in flash loader demo program.
please give me stmap file or please let me konw how to modify with other stmap file.
thanks a lot.
Solved! Go to Solution.
2018-12-26 4:23 PM
The files are ASCII, and there are multiple examples of form/function.
The tool is deprecated, use the STM32 Cube Programmer in UART/COM mode.
https://www.st.com/en/development-tools/stm32cubeprog.html
2018-12-26 4:23 PM
The files are ASCII, and there are multiple examples of form/function.
The tool is deprecated, use the STM32 Cube Programmer in UART/COM mode.
https://www.st.com/en/development-tools/stm32cubeprog.html
2018-12-26 4:43 PM
hello,
thanks for your reply. where can i get this file? i cannot see any example of form.
please let me know the web link.
i also installed the stm32 cube programmer. but i cannot see stmap file that is related with stm32l433. i see only html file.
i make pc program like as flash loader demo program for mass production . so, i need stmap file for my pc program.
however, this file format is below like that
;;******************** (C) COPYRIGHT 2014 STMicroelectronics ********************
;;* File Name : STM32_Med-density_128K.STmap
;;* Author : MCD Application Team
;;* Version : V2.7.0
;;* Date : 15-September-2014
;;* Description : memory mapping
;;********************************************************************************
;;* THE PRESENT SOFTWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS
;;* WITH CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO SAVE TIME.
;;* AS A RESULT, STMICROELECTRONICS SHALL NOT BE HELD LIABLE FOR ANY DIRECT,
;;* INDIRECT OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY CLAIMS ARISING FROM THE
;;* CONTENT OF SUCH SOFTWARE AND/OR THE USE MADE BY CUSTOMERS OF THE CODING
;;* INFORMATION CONTAINED HEREIN IN CONNECTION WITH THEIR PRODUCTS.
;;********************************************************************************
[Product]
Name=STM32_Med-density_128K
PID=0410
FlashSize=0080 ;;ADDR_FLASH_SIZE=1FFFF7E0;
RAMSize=0014
PacketSize=80
ACKVAL=79
MAPNAME=Pages
PagesPerSector = 4
family = 1;
[Page0]
Name=Page0
Index=00
Address=08000000
Size=00000400
Type=111
UFO=111
[Page1]
Name=Page1
Index=01
Address=08000400
Size=00000400
Type=111
UFO=111
[Page2]
Name=Page2
Index=02
Address=08000800
Size=00000400
Type=111
UFO=111
[Page3]
Name=Page3
Index=03
Address=08000C00
Size=00000400
Type=111
UFO=111
[Page4]
Name=Page4
Index=04
2018-12-26 6:14 PM
>>i make pc program like as flash loader demo program for mass production
Ok, so wouldn't the Reference Manual and Data Sheet sufficiently describe the memory map and flash sectors sizes for the mechanics of that to continue to work?
Pick an L4 example, it will be a shorter walk. STM32L4x_6_1024K.STmap
2018-12-26 9:31 PM
hello.
i got the STmap file from other way. thanks for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.