2018-01-09 2:43 AM
Hello,
I have a problem with my bootloader. At the first launch I write a 64 bit word in flash in 0x8004030. I was able to check with J-Mem to make a dump of the memory and it flash writing OK.
If I read the value at this address in 0x8004030 there is 0xfffffffff.
In assembler I have:ldr r2, [r5, # 0]R5 = 0x8004030and the result in R2 is 0xffffffff wich is wrong.And if I read the value at this address in 0x00004030 there is good value.
why there is not the same value in 0x08004030 when 0x00004030?
Thanks,
Eric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.