cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L412 Nucluo64 - garbage data sent from UART

simo zz
Senior II

Hello,

I am working with the evaluation board STM32L412 Nucluo64, but I noticed that the MCU sends only garbage from UART.

The code I am using has been used many times in other projects and should work fine (it's just a matter of calling LL_UART_TransmitData8 and wait for transfer complete).

Just tested on a STM32L4 Nucleo (STM32L432KC), same setup for both boards and works fine.

Do someone has an idea of what could be wrong ?

Thanks.

s.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Are you sure it uses a 25 MHz XTAL? Should use 8 MHz from ST-LINK or 32.768 KHz from LSE XTAL

Check HSE_VALUE define, and if you're using the MSI or HSI clock sources.

Availability and quality of baud rates will depend on available source clock.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

6 REPLIES 6

Hello

STM32L412 NUCLEO uses 8 MHZ Clock from STLink as HSE

STM32L432KC NUCLEO uses 25 MHZ XTAL osc

Are you sure it uses a 25 MHz XTAL? Should use 8 MHz from ST-LINK or 32.768 KHz from LSE XTAL

Check HSE_VALUE define, and if you're using the MSI or HSI clock sources.

Availability and quality of baud rates will depend on available source clock.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
simo zz
Senior II

Hello @Vangelis Fortounas​ ,

I think I don't understand at all your reply.

Nucleo64 jumper SB64 is open by default

0693W000006FenmQAC.png0693W000006FerJQAS.png 

The schematic correctly represents the real hardware connection.

HSI clock @16 MHz can be used with the PLL and getting a wide range of sys clock frequencies, smaller or greater than 25 MHz.

Using LL drivers, once set up the oscillator, the baudrate divider is automatically calculated into the function

LL_USART_SetBaudRate

called from

LL_USART_Init

What should be the difference from one clock frequency to another if both can achieve a correct divider for baudrate = 115200 ?

Thanks.

s.

MSI clock seems to work fine.

Thanks fot the hint.

s.

Hello, I was completely wrong about clocks. ( checked wrong schematics)

Hello .About the clocks , i was wrong(checked wrong schematics).

> What should be the difference from one clock frequency to another if both can achieve a correct divider for baudrate = 115200 ?

The difference is in the the Freq drift over the whole temperature range.

The most accurate clock source has the less probability to produce Frame Errors

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.