2021-04-17 2:12 AM
Hello,
I run into problem for selecting TIM2 as my pwm output. As it turns out, it is only output capable. But I need to get processor independent 3kHz 50:50 PWM signal with no AF functional PWM.
Any simple idea how can I toggle with 50% 3kHz duty cycle this GPIO? (PA15 on STM32L412C8)
I Am thinking of using DMA, just have no idea how to do that, since I can't use ODR register,I have multiple pins that should not change, and with BRR BSRR, well, it is two address, so what ? Do ping pong DMA with single transfer and circular buffer ?
Any ideas are welcome :)
Solved! Go to Solution.
2021-04-17 5:45 AM
Hi,
I found the problem, I was looking at LPTIM2 instead of TIM2
No problems in this case :) Thank you all !
2021-04-17 2:22 AM
PA15 is TIM2_CH1and can do PWM . All other solutions wll give you at least Jitteror even missing cycles.
2021-04-17 4:34 AM
First, like Uwe already said...
Second, read what a BSRR register is. At least read it's name!
2021-04-17 5:45 AM
Hi,
I found the problem, I was looking at LPTIM2 instead of TIM2
No problems in this case :) Thank you all !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.