2019-08-09 3:11 AM
Hi, I'm using the STM32L073CZ micro in a thermometer application.
I've used CubeMX to create the base code and adapted it.
I'm using ADC channel 1 for the temperature measurement, which is working correctly. I'm only initializing the ADC channel when its needed and then de-Initializing it after using HAL_ADC_DeInit(&hadc);
I'm also doing a battery voltage calculation using ADC channel 7 along with the internal reference measured on ADC channel 17. This is initialized with its own function.
This function is also working but......
When i de-Initializing it though i don't think i'm un-configuring the internal ref channel, which is causing an additional drain on the battery.
Please ask for any addition info.
Thanks in advance.
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.