cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L053DISCO - How to enable 3V_O or 5V_O

Thomas L.
Associate III

In the document UM1775 there is stated the following:

"5 V and 3 V can be used as output power supplies when an extension board is

connected to pins P2 and P3.

...

In this case, the 5V_O and 3V_O pins deliver a 5 V or 3.3 V power supply and the

power consumption of the extension board must be lower than 100 mA."

Yet, the Supply for 3V_O is gated through T2 which in turn is controlled by PB15 on the SM32F103 (PWR_ENn); I guess that this is the controller which handles the ST-Link and cannot be changed.

How does this controller determine if there is an extension board connected to P2 or P3 so that it enables that supply?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

PWR_ENn enables power to the whole board, including the target, when the STLink sucessfully enumerates (or if this is overriden using the JP2 jumper).

Note, that 3V_OUT is shorted to 3V3.

JW

View solution in original post

2 REPLIES 2
waclawek.jan
Super User

PWR_ENn enables power to the whole board, including the target, when the STLink sucessfully enumerates (or if this is overriden using the JP2 jumper).

Note, that 3V_OUT is shorted to 3V3.

JW

Thomas L.
Associate III

Oh I see. Thanks, that makes sense

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.