2020-08-21 1:11 PM
I have a STM32L031K6 Nucleo Board...
I want to use the DWT.. but I become this errors:
../Core/Src/../Inc/stm32_delay.h:35:30: error: 'DWT' undeclared (first use in this function)
uint32_t clk_cycle_start = DWT->CYCCNT;How can I Use DWT or Enable it? I Use STM32CubeIDE...
My Function:
#ifndef INC_STM32_DELAY_H_
#define INC_STM32_DELAY_H_
#ifdef __cplusplus
extern "C" {
#endif
#ifndef __STM32L0xx_HAL_H
#include "stm32l0xx_hal.h"
#endif
/**
* @brief Initializes DWT_Cycle_Count for DWT_Delay_us function
* @return Error DWT counter
* 1: DWT counter Error
* 0: DWT counter works
*/
uint32_t DWT_Delay_Init(void);
/**
* @brief This function provides a delay (in microseconds)
* @param microseconds: delay in microseconds
*/
__STATIC_INLINE void DWT_Delay_us(volatile uint32_t microseconds)
{
uint32_t clk_cycle_start = DWT->CYCCNT;
/* Go to number of cycles for system */
microseconds *= (HAL_RCC_GetHCLKFreq() / 1000000);
/* Delay till end */
while ((DWT->CYCCNT - clk_cycle_start) < microseconds);
}
#ifdef __cplusplus
}
#endif
#endif /* INC_STM32_DELAY_H_ */Thanks guys..
Solved! Go to Solution.
2020-08-21 1:56 PM
Pretty sure the L031 lacks any 32-bit timer, ST not really understanding expectations for 32-bit processors in this regard.
Sharper engineers would have put in at least a 32-bit counter, dealing with the critical-path/propagation issues, and built a less complex assortment of timing units..
2020-08-21 1:19 PM
No CM0(+) doesn't have this, adds too many transistors.
You'll need to do timing via a free-running 16-bit (or 32-bit if available) TIM
You can set the TIM prescaler such that it counts micro-seconds, or processor cycles.
Period = 0xFFFF, or 0xFFFFFFFF
Use TIMx->CNT to observe passage of time
2020-08-21 1:33 PM
Hello,
Thank you, okay, I am really new to stm32 and come from Atmel/Microchip development.
I there a example to use a TIM (32 bit available) as a micro-seconds counter? ;)
2020-08-21 1:49 PM
__STATIC_INLINE void TIM_Delay_us(uint16_t microseconds)
{
uint16_t clk_cycle_start = TIM2->CNT;
/* Go to number of cycles for system */
microseconds *= (HAL_RCC_GetHCLKFreq() / 1000000);
/* Delay till end */
while ((TIM2->CNT - clk_cycle_start) < microseconds);
}
Doing this blind, something like this to set up
TIM_HandleTypeDef TimHandle;
/* TIMx Peripheral clock enable */
TIM2_CLK_ENABLE();
/* Set TIMx instance */
TimHandle.Instance = TIM2;
TimHandle.Init.Period = 0xFFFF; // MAXIMAL 16-bit
TimHandle.Init.Prescaler = 0; // DIV1
TimHandle.Init.ClockDivision = 0;
TimHandle.Init.CounterMode = TIM_COUNTERMODE_UP;
if (HAL_TIM_Base_Init(&TimHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/* Start Timebase */
if (HAL_TIM_Base_Start(&TimHandle) != HAL_OK)
{
/* Starting Error */
Error_Handler();
}
2020-08-21 1:56 PM
Pretty sure the L031 lacks any 32-bit timer, ST not really understanding expectations for 32-bit processors in this regard.
Sharper engineers would have put in at least a 32-bit counter, dealing with the critical-path/propagation issues, and built a less complex assortment of timing units..
2020-08-21 2:06 PM
Hello!
Thanks, I have 1 TIM available, and I need a usDelay Timer for a SPI strobe...
then I must use a 16-bit Timer...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.