2022-03-04 1:04 AM
In a previous project, I configured the PA0, PA1 PA2 inputs as ADC and read them with DMA without any problems. Since I need to use PA0 and PA1 for another job, I shifted the ADC inputs to PA7 and PB1. but I was not able to read these channels with DMA. Is there a limitation of L0 series with ADC and DMA that I am not aware of?
2022-03-04 5:33 AM
> Is there a limitation of L0 series with ADC and DMA that I am not aware of?
The DMA doesn't care (or know) about what pins you're using. ADC results are placed in ADC->DR regardless of the pin used and the DMA picks them up from there.
Must be another bug somewhere.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.