2015-11-06 10:48 AM
Interrupt is working good when STM is in run mode, but when STM enter STOP mode interrupt from pin PC12 doesn't work, end after that interrupt doesn't work at all, even when STM enter run mode againt. It's seems like sleep somehow kill this interrupt.
This is my initialization: /*Configure GPIO pin : PC12 */ GPIO_InitStruct.Pin = GPIO_PIN_12; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); HAL_NVIC_SetPriority(EXTI4_15_IRQn, 1, 0); HAL_NVIC_EnableIRQ(EXTI4_15_IRQn);void EXTI4_15_IRQHandler(void){ / USER CODE BEGIN EXTI4_15_IRQn 0 / / USER CODE END EXTI4_15_IRQn 0 / HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_12); / USER CODE BEGIN EXTI4_15_IRQn 1 / / USER CODE END EXTI4_15_IRQn 1 /} void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin){ if (GPIO_Pin == GPIO_PIN_12){ WakeUpFromISRChargerTrigger(); UpdatePocketFinderStatus(); }}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.