2013-06-04 10:47 PM
Hi!
I'm using STM32L152 + IAR6.5. EEPROM writing/erazing routings are placed in RAM. Interrupt vector table and critical interrupt handler too. I need to write EEPROM and serve critical interrupt at the same time. Before writing to the EEPROM all interrupts are disabled excepting one critical. This approach works perfectly. I've checked critical interrupt presence by scope during EEPROM writing and EEPROM content afterwards. Then I added USB VCP driver provided by ST. I've discovered that program was stalled during EEPROM writing. Critical interrupt doesn't appear at this time. Why? USB interrupts are disabled before EEPROM writing. How can USB driver affects to the memory bank? Any ideas are welcome. Thanks.2013-06-05 10:52 AM
Are you working on STM32_USB-FS-Device_Lib_V4.0.0 (STSW-STM32081) ?
The default Suspend/Resume behavior of the USB device stack may disturb your process, as discussed on topic. The Suspend() code (in usb_pwr.c) of this stack drops the entire system into STOP mode. By this code, the device stays in STOP mode, while USB is not plugged in, and until bus reset occurs on USB after plug in. Temporarly, drop CNTR_SUSPM and CNTR_ESOFM from IMR_MSK() definition in usb_conf.h, as described on above post, to disable this behavior. Tsuneo2013-06-05 11:28 PM
Hi!
Thank you so much. It works as assumed now! Yes, I'm using STM32_USB-FS-Device_Lib_V4.0.0. I know about Suspend, I tried to prevent going to Suspend by setting __IO bool fSuspendEnabled = FALSE; /* true when suspend is possible */ and I thought that it's OK. The device shouldn't going to low power mode at this stage of development and has to operate without USB plugging.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.