2021-11-19 4:57 PM
Hello All,
I have an intresting issue that came up. But I am not sure if I understand it. In the clock configurator, I gave the usart mux a 100Mhz clock for the uarts and set up the baud rate for 115200K. Once I started sending data, I noticed that the baud rate was off. I went back and gave the clocking mux 64mhz, and that seemed to fix that issue. I want to make sure I understand why this before I move forward. Any advice would be greatly appreciated.
Solved! Go to Solution.
2021-11-20 1:08 AM
Check the clock signal on the board as built, pretty sure it clocks at 8 MHz from the ST-LINK/V2-1
2021-11-19 5:34 PM
>>STM32HT43 Nucleo 144
?? WHAT?
You mean an STM32H743ZI2 board ? The ZI2 board has a slightly off-frequency HSE clock, the ST-LINK/V3 is 8.33 MHz, not 8 MHz of the older ZI board
Check that HSE_VALUE is consistent with the source clock.
The 64 MHz HSI clock is likely closer to nominal.
2021-11-19 11:37 PM
oops STM32H743ZI Nucleo 144 typo, sorry. The schematic is saying the HSE input clock is 25 MHz for that board. Should I measure the 25 MHz clock? Getting a bit concerned as I am getting ready to work with CAN FD. I am using PLL1Q for that which is derived from the HSE clock.
2021-11-20 1:08 AM
Check the clock signal on the board as built, pretty sure it clocks at 8 MHz from the ST-LINK/V2-1
2021-11-20 1:10 PM
When you update the ST-LINK firmware with a recent version, there will be two options for the clock to the MCU: 8.33... (HSE/3) and 8.0 (HSI/2 of 'F7)
2021-11-20 2:49 PM
Please forgive me as I am confused about the stlink clock and the HSE clock on the MCU. They are two different devices. How would this affect the baud rate on the MCU?
2021-11-20 3:18 PM
To save parts the on-board ST-LINK can provide a crystal based clock source to the target MCU
Review schematic
2021-11-20 3:52 PM
The ST-LINK MCU on the Nucleo board (STM32F7) has a 25 MHz crystal connected to its HSE. It's MCO goes to the target MCU's HSE in "bypass" (single-ended) mode. Several clocks can be muxed to the MCO, with programable divisor.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.