cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743I-EVAL

kerry woodbury
Associate
Posted on March 19, 2018 at 22:06

I am trying to run some of the test code in the STM32Cube Package for the H7 v1.2, within IAR, however, I am unable to download and debug the example programs.  I have tried both a J-Link and the on board ST-Link hardware.  Unable to determine if this is a hardware or software issue at this point.  Please let me know if you have any suggestions.  Thanks!  Kerry

#stm32h7
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on March 20, 2018 at 15:55

You should try the ST-LINK Utilities and test the on-board ST-LINK.

Board here works fine with Keil, suggest you download an evaluation of that and build some of the demo projects supplied in the HAL examples under the CubeH7 trees.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
kerry woodbury
Associate
Posted on March 20, 2018 at 16:31

I finally traced this issue to the IAR flashloader.  If I use the J-Link Flashloader then the program can be downloaded to the flash.  The IAR flashloader  ($TOOLKIT_DIR$\config\flashloader\ST\FlashSTM32H7xxx_CM7.board) needs to be corrected/changed.  If anyone has an updated IAR flashloader file for the STM32H743I-EVAL please share.  Thanks!  Kerry

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.