2026-01-16 11:01 AM - last edited on 2026-01-17 1:14 PM by mƎALLEm
Im trying to drive 3.5 inch TFT LCD with STM32H743 using FMC. My setup is :
My timing settings are (FMC Clock: 10Mhz):
Here are the parts of code:
When I try to write a data, as shown in the attachment, my logic analyzer shows me multiple WR event occured and shows some weird signals on data line (D0-D3).
I do not understand where I did wrong...
Solved! Go to Solution.
2026-01-17 1:12 PM
Hello,
To drive LCDs through FMC with MCUs with Cortex-M7 you need to configure the LCD memory region in Strongly-Ordered or Device configuration using the MPU.
2026-01-17 1:12 PM
Hello,
To drive LCDs through FMC with MCUs with Cortex-M7 you need to configure the LCD memory region in Strongly-Ordered or Device configuration using the MPU.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.