2024-07-31 2:32 AM
Hello,
I am currently trying to setup a timer to measure time in between two pulses. I have managed to get it working with the code below but the issue is that I get very imprecise readings on the frequency. I get an error that is hovering around 1-1.5%, what can I do to minimize this error or is it not possible to get less then 1% error in this type of reading?
(The setting in values is done within the init function. I just dont want to send the whole code base)
Regards,
Björn
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim){
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_3)
{
if (Is_First_Captured==0) // if the first rising edge is not captured
{
IC_Val1 = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_3); // read the first value
Is_First_Captured = 1; // set the first captured as true
}
else // If the first rising edge is captured, now we will capture the second edge
{
IC_Val2 = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_3); // read second value
if (IC_Val2 > IC_Val1)
{
Difference = IC_Val2-IC_Val1;
}
else if (IC_Val1 > IC_Val2)
{
Difference = (0xffff - IC_Val1) + IC_Val2;
}
float refClock = TIMCLOCK/(PRESCALAR);
frequency = refClock/Difference;
__HAL_TIM_SET_COUNTER(htim, 0); // reset the counter
Is_First_Captured = 0; // set it back to false
}
}
}
uint32_t IC_Val1 = 0;
uint32_t IC_Val2 = 0;
uint32_t Difference = 0;
int Is_First_Captured = 0;
/* Measure Frequency */
float frequency = 0;
#define TIMCLOCK 270000000
#define PRESCALAR 1375
htim23.Instance = TIM23;
htim23.Init.Prescaler = 1374;
htim23.Init.CounterMode = TIM_COUNTERMODE_UP;
htim23.Init.Period = 4294967295;
htim23.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim23.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;
sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;
sConfigIC.ICFilter = 0;
2024-08-01 7:22 AM
So your input signal has ~ 16 mHz to 1 Hz, then the timer resolution at now 100 kHz (?) should be good enough.
But at these low frequencies, do you really have a stable signal source? It should not be a problem, but I would check the generator specs.
So better try TDK's idea and check with your own PWM.
And again, check the raw integer values that you get.
2024-08-01 7:31 AM - edited 2024-08-01 7:31 AM
I am not to familiar with reading stability of generators but according to our picoscope the signal is very stable and the frequency is correct. The generator is a TG550 from AIM-TTi.
2024-08-01 8:49 AM
Sure you can simply trust your generator and scope (I would not at that low frequency).
Generator specs:
Frequency:
Auto-ranging reciprocal measurement giving
4 digit resolution for frequencies down to
1Hz; maximum resolution is 0.001Hz.
Accuracy ±1 digit 0.2Hz to 5MHz; accuracy
±1% of range full scale below 0.2Hz
I haven't found any jitter specs that quick.
I would build my own PWM signal, as TDK proposed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.