2024-11-27 10:40 PM
Hi,
My test board can enter sleep mode OK, but doesn't wake up when PC13 goes high: (never reach __enable_irq())
void Sleep() {
__disable_irq();
SysTick->CTRL = 0;
// Enable WKUP4 (PC13)
PWR->WKUPEPR = PWR_WKUPEPR_WKUPEN4; // Enable WKUP4
PWR->WKUPCR = 0xFFFFFFFF; // Clear all wake-up flags
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
PWR->CR1 |= PWR_CR1_LPDS; // Low Power Deep Sleep
__DSB();
__ISB();
__WFI(); // Enter deep sleep
__enable_irq();
}
2024-11-28 2:15 AM
Hello @harareyd, welcome to the ST community,
Consider using __WFE() instead of __WFI() to enter sleep mode. The __WFE() instruction can be more suitable for event-driven wake-up scenarios.
But your code is correct... maybe the issue is with the physical button! could you test it?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-28 2:35 AM
I am not much oriented in sleep modes, but it looks like you go to sleep with disabled interrupts.
2024-11-28 9:15 AM
When using __WFE() the board doesn't enter sleep mode at all unfortunately. It just skips right over the __WFE() instruction. I verified that the input is working. Sleep() is called when PC13 goes low.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.