2025-10-29 7:57 AM
Hi everyone,
I’m trying to generate a square wave using TIM5 Output Compare (OC) on an STM32H7 board. I configured TIM5_CH1 to output on PA0, both in CubeMX and manually in HAL_TIM_MspPostInit(). Here is a snippet of my GPIO init:
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF2_TIM5;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);And the TIM5 channel configuration:
sConfigOC.OCMode = TIM_OCMODE_TOGGLE;
sConfigOC.Pulse = 3749;
HAL_TIM_OC_ConfigChannel(&htim5, &sConfigOC, TIM_CHANNEL_1);
The problem is that the square wave always appears on PA1, not PA0, even though I haven’t configured TIM5_CH2 anywhere.
I checked the datasheet pin mapping:
PA0 → TIM5_CH1
PA1 → TIM5_CH2
PA2 → TIM5_CH3
PA3 → TIM5_CH4
I suspect this might be related to alternate function routing or some hardware conflict on PA0 (maybe boot/debug pins), but I’m not sure.
Has anyone seen this behavior on STM32H7? What could cause TIM5_CH1 output to be redirected from PA0 to PA1?
Thanks in advance!
2025-10-29 8:06 AM
> an STM32H7 board
Which board? Which chip? Consult the schematic. Probably PA0/PA1 have been mismatched somehow.
> What could cause TIM5_CH1 output to be redirected from PA0 to PA1?
Nothing will cause this; the problem is elsewhere. The code you showed will initialize PA0. No problems there.
2025-10-29 8:31 AM - edited 2025-10-29 8:33 AM
Thank you for your answer.
> Which board?
STM32 Nucleo-144 development board with STM32H743ZI2 MCU
I’m not sure if it’s a user-related issue. As I mentioned, the situation is the same on different channels, and no matter which pin I initialize, the output always appears on pa1.
2025-10-29 9:18 AM - edited 2025-10-29 9:21 AM
Hello,
Please share your ioc file or even your complete project and what CubeMx version are you using?
2025-10-29 9:31 AM
Also share what pin you're measuring the signal on with a picture. Probably just using the wrong pin and/or it's mislabeled in the reference you're using.
2025-10-29 9:32 AM
> As I mentioned, the situation is the same on different channels, and no matter which pin I initialize, the output always appears on pa1.
Probably you are not running the code that you think you're running.
2025-11-04 1:48 AM
Sorry for the late response — I couldn’t share the project, and I’ve only recently had time to look into this again.
Even when I don’t configure or start any timer, PA1 still seems to output some kind of signal. Since I don’t have access to an oscilloscope or other measurement tools, I tried to analyze it in software instead.
I connected PA1 to another pin configured as an EXTI input (rising edge) and measured interrupt timing using the DWT_CYCCNT counter to understand the signal behavior. If my approach and interpretation are correct, the interrupt triggers very consistently in the microsecond range, suggesting that PA1 is indeed toggling or outputting something.
I realize the board itself is unlikely to be faulty, and unfortunately, I don’t have a spare one to cross-check. So I’m just trying to understand what might cause this — whether it’s something I’ve overlooked or a mistake on my end.
CubeMX version is 1.18
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.