2021-02-25 5:29 AM
Hi,
I am using SPI1 and interrupt are enabled in this function
void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{
........................
/* SPI1 interrupt Init */
HAL_NVIC_SetPriority(SPI1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SPI1_IRQn);
/* USER CODE BEGIN SPI1_MspInit 1 */
/* USER CODE END SPI1_MspInit 1 */
}Spi works fine in blocking mode, I want to switch to DMA mode but I never enter this function :
void SPI1_IRQHandler(void)
{
/* USER CODE BEGIN SPI1_IRQn 0 */
/* USER CODE END SPI1_IRQn 0 */
HAL_SPI_IRQHandler(&hspi1);
/* USER CODE BEGIN SPI1_IRQn 1 */
/* USER CODE END SPI1_IRQn 1 */
}Any ideas why my interrupts are never triggered ?
Gabriel
2021-02-25 5:48 AM
Hello.
Is not enough to enable SPI global interrupt.
Need to enable also a particular bit of SPI like TXEIE for empty TX buffer , RXNEIE for incomming data, etc.
__HAL_SPI_ENABLE_IT(&hspi1, SPI_IT_RXNE) ;
2021-02-25 6:08 AM
Thanks, I added
static void mySPI1_Init(void)
{
...............
HAL_SPI_Init(&hspi1);
__HAL_SPI_ENABLE_IT(&hspi1, SPI_IT_EOT) ;
}But I still never go into SPI1_IRQHandler() :sad_but_relieved_face:
I want to use :
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
2021-02-25 3:18 PM
Hello:)
End of Transmision interrupt implies that a byte is clocked out before, SPI is enabled and configured properly.
To have HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi) called , HAL_SPI_Receive_DMA(..) or HAL_SPI_Receive_IT(..) must called first.
There are some working examples for SPI inside repository. C:\Users\you\STM32Cube\Repository
This document contains HAL SPI explanations for every function , structures and how to use it.
2021-02-26 1:57 AM
My transfert gets triggered here, I checked with debugger and I get into this function (ads_buf is located in D2 RAM with MPU region in WT)
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
if((GPIO_Pin == DRDY_ADC_Pin)&&(data_flag))
{
ADS1x9x_csn_0_en();
//HAL_SPI_Receive(&hspi1, ads_buf, READBACK_LENGTH,500);
HAL_SPI_Receive_DMA(&hspi1, ads_buf, READBACK_LENGTH);
}
}But I dont go into this one
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{My spi1 handler says :
RxXferSize = 27 and RxXferCount = 27 so the Rx is completed
pRxBuffPtr is 0x30000000 so right in my D2 RAM buffer
state is HAL_SPI_STATE_BUSY_RX
My DMA state is HAL_DMA_STATE_BUSY
My buffer doesn't get written, any ideas why it can't ?
2021-02-26 2:38 AM
I have the same problem when using IT function, I receive the message but never trigger any interrupt
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.