2021-08-06 4:31 AM
I have difficulties with the following scenario:
There is a big buffer of bytes in DTCM memory. The buffer should be transmitted out through UART or SPI. I'm looking for solution, where software only configures the transaction, and then the whole process is done by hardware automatically.
As DMA1/2 cannot work with DTCM, we need to use MDMA.
The simplest implementation is as follows:
Unfortunately, there are gaps in this scheme:
If anybody knows solution, or can point out relevant example, any help will be highly appreciated.
2021-08-06 5:33 AM
Maybe you need correct subject to MDMA - DMA .
And because UART or SPI is slower as MDMA, is ideal oposite way DMA will request MDMA on half and full IRQ complete.
And i mean without some IRQ code your idea dont will work as complete offload MCU.
2021-08-06 6:30 AM
>> Maybe you need correct subject to MDMA - DMA .
Sorry, I didn't catch your point.
>> And i mean without some IRQ code your idea dont will work as complete offload MCU.
So, you consider the hardware cannot acomplish this work without software assist.
Maybe; however MDMA seems rather close to this purpose. Probably, very simple additions to the hardware would provide support of this scenario and many other useful scenarios.
2021-08-06 12:25 PM
There's no way to chain MDMA and DMA like this without any intervention of the CPU. Note practically, at least. You could do awkward things with timers triggering the DMA transfers.
If you can't devote even 20-30 ticks to start the DMA after MDM is complete, a simple solution would be to use SRAM2 instead of DTCM.
2021-08-06 12:45 PM
Thank you, guys.
Software-assisted solution was implemented before.
Simply looking for better solution.
2021-08-23 7:05 AM
It seems that mdma linked list is made for that purpose, as you said in your first post. It's a little bit cumbersome to write all the mdma blocks, but it will work without cpu intervention. I use that solution in a project, but had to resolve a problem on the trigger event to load next linked mdma block. I have found workaround, first software assisted, then hardware assisted, but it still look hackish, more details here : https://community.st.com/s/question/0D53W00000xsRELSA2/mdma-linked-list-unconditionnal-trigger-to-next-block
2021-08-23 8:35 AM
Thank you Alexandre.
Your solution is really sharp. However, you are correct, it looks like a hack.
For a while, I can live with software-assisted solution.
Actually, I have impression that MDMA, although sophisticated, is a bit raw. With addition of relatively simple hardware, it would be able to support many useful scenarios that currently are not avilable or require awkward hacks.
Few simple additions are evident:
2021-08-31 12:09 AM
It seems that mdma connected list is made for that purpose, as you said in your first publish. It's a little bit cumbersome to write down all the mdma blocks, but it will work without CPU intervention. I use that answer in a challenge, but needed to solve a hassle on the cause event to load subsequent related mdma block.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.