2022-04-13 12:39 AM
Hi.
It seems, that sometimes data in cached memory is corrupted.
DMA transfer data from SPI to SRAM2 (0x30000000). I use ping-pong buffer in SRAM2 (two similar buffers). Data processing performing for first part of the buffer in thread, while second it's part is filled with data over DMA.
DMA write 35 bytes to buffer. DMA start next time and write to next 35 bytes and so on 72 times. After 35*72 bytes are written into first part of the ping-pong buffer, it swap to second part. Both parts are 35*72 bytes.
Both start address of buffer parts are alligned to 32 bytes (but size of buffer is not alligned to 32 and accsess from thread is one byte alligned).
Of course invalidate cache before processing is performed. Buffer part for thread (35*72 bytes) is invalidated. But sometimes data in buffer seems is not valid.
Usually failed data that correspond one DMA transaction (all 35 bytes), but one or some corrupted bytes meet too.
When cache is disabled there is no one error for very long period of time. When cache is enabled error rates is about 1e-6. It is too much for my application.
Additional considerations
Do you have any suggestions?
Regards, Aleks.
Solved! Go to Solution.
2022-04-13 5:13 AM
> but size of buffer is not alligned to 32 and accsess from thread is one byte alligned
Then align the size also. In your case 35*72=2520 B. The closest aligned size is 2528 B. You don't have to use those 8 bytes but they have to be there so that they take up the space and invalidation doesn't damage other variables. One can afford wasting 2*8 bytes on H7 series.
> Of course invalidate cache before processing is performed.
Invalidation must be done before passing the buffers to the DMA - before the reception on a particular buffer is started. Doing it after the reception is too late and is a flaw. The reason is a cache eviction process.
Read my comment carefully:
Detailed example of cache eviction:
https://community.st.com/s/question/0D50X0000C9hGozSQE/weird-cache-writeback-behavior-for-stm32f7508
2022-04-13 5:13 AM
> but size of buffer is not alligned to 32 and accsess from thread is one byte alligned
Then align the size also. In your case 35*72=2520 B. The closest aligned size is 2528 B. You don't have to use those 8 bytes but they have to be there so that they take up the space and invalidation doesn't damage other variables. One can afford wasting 2*8 bytes on H7 series.
> Of course invalidate cache before processing is performed.
Invalidation must be done before passing the buffers to the DMA - before the reception on a particular buffer is started. Doing it after the reception is too late and is a flaw. The reason is a cache eviction process.
Read my comment carefully:
Detailed example of cache eviction:
https://community.st.com/s/question/0D50X0000C9hGozSQE/weird-cache-writeback-behavior-for-stm32f7508
2022-04-13 6:26 AM
Invalidate the first half of the buffer after it's received but before you read it. Do the same with the second half. Do not globally invalidate the cache as this causes other issues. You will need to align each half of the buffer to fit cleanly within a cache page.
2022-04-13 12:27 PM
I am sorry for my unclear note. The sizeof(buffers) is not aligned to 32 byte, but addresses of all buffers for DMA are aligned to 32 bytes. So it is OK.
I am confused with your suggestion
> Invalidation must be done before passing the buffers to the DMA - before the reception on a particular buffer is started
because https://www.st.com/resource/en/application_note/dm00272913-level-1-cache-on-stm32f7-series-and-stm32h7-series-stmicroelectronics.pdf After the DMA transfer complete, when reading the data from the peripheral, the software must perform a cache invalidate before reading the DMA updated memory region.
And I do it exactly. But will read your materials and try correspond it.
2022-04-13 12:28 PM
Exactly this is done.
2022-04-13 11:30 PM
It seems that reason in sequential read and write to buffer by means of my code, i. e. CPU read modify and write data to cachable buffer.
I suppose there are possible issues:
I remove writing to buffer and errors are disapier with other equal conditions.
DSB instructions after RD, WR operations do not resolve the problem.
for (size_t cnt = 0; cnt < lenBuf; ++cnt)
{
// crc check
uint32_t *ptr = reinterpret_cast<uint32_t *>(&(bufRd[cnt][1])); // byte 1 - dummy
uint32_t len = static_cast<uint32_t>(Mcp3914::lenCrcSpiPart); // adc data
uint32_t crcCalculated = HAL_CRC_Calculate(phcrc, ptr, len); // CRC16
uint16_t crc16; // CRC16 for SPI frame
crc16 = bufRd[cnt][Mcp3914::lenBufDmaSpi - 2] << 8;
crc16 |= bufRd[cnt][Mcp3914::lenBufDmaSpi - 1];
uint16_t *crcIsInvalid = reinterpret_cast<uint16_t *>(&(bufRd[cnt][Mcp3914::lenBufDmaSpi - 2]));
// place crc status to "crc16" field
*crcIsInvalid = crc16 ^ static_cast<uint16_t>(crcCalculated);
// to little endian data
int32_t *pAdcData;
int32_t littleEndianData;
for (size_t ch = 0; ch < Mcp3914::channelsTotal * Mcp3914::lenChannelAdc; ch += Mcp3914::lenChannelAdc)
{
pAdcData = reinterpret_cast<int32_t *>(&bufRd[cnt][ch + 1]);
littleEndianData = static_cast<int32_t>(__REV(*pAdcData));
*pAdcData = littleEndianData;
}
}Here bufRd is DMA buffer.
There is no one error if cache is disabled for SRAM buffer.
Why invalidating full cache resolve the problem?
Kind regards, Aleks.
2022-04-18 2:50 AM
Hi Piranha!
I read carefully your comments in the topic. I invalidate buffers before start accept data from DMA and after receiving is completed. Problem is seems solved.
Yes, even for receive part the invalidation must be done before passing buffers to DMA, because otherwise cache eviction can damage the receive buffers by writing back dirty lines during reception.
So invalidate must be done before start receiving and after receiving is comleated.
Thank you for responce.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.