2026-02-27 2:23 AM - last edited on 2026-02-27 4:17 AM by mƎALLEm
A new STM32 sub-family (as part of the 'H5 family) came out. They have everything but the kitchen sink. As far as I can tell, 'H5E4 and 'H5E5 differ only in that the higher one has USB-HS with PHY (the 'H5Fx are crypto-enabled variants, as usually)
What's new is also the PLAY peripheral, which is a small programmable logic element, fully documented and configurable through registers. It's based around 16 simple logic elements (4-input LUT and an optional register), complete with an extensive input multiplexer matrix+filter, interconnected to a variety of peripherals (timers, DMA, ADC...) and also GPIO.
I wonder, if there's a Disco around...
JW
Solved! Go to Solution.
2026-02-27 3:21 AM - edited 2026-02-27 3:50 AM
Hello,
@waclawek.jan wrote:
I wonder, if there's a Disco around...
JW
There will be one Discovery board and one NUCLEO board ;).. Stay tuned.
You can use the latest version of CubeMx and use the board selector:
2026-02-27 2:54 AM - edited 2026-02-27 3:12 AM
I don't see the PLAY mentioned on the STM32H5E4/5F4 or STM32H5E5/5F5 pages ?
PS:
But I do see it in DS14972 (STM32H5Fxxx) and RM0517 (STM32H5E4/5F4 and STM32H5E5/5F5), both at Rev 1.
Haven't checked any others yet ...
2026-02-27 3:06 AM
Thanks for the info, very interesting.
Just checking the RM.
Could be a few more gates and FFs for me to replace a Spartan 6 ... :D
But going into the right direction for my taste!
2026-02-27 3:21 AM - edited 2026-02-27 3:50 AM
Hello,
@waclawek.jan wrote:
I wonder, if there's a Disco around...
JW
There will be one Discovery board and one NUCLEO board ;).. Stay tuned.
You can use the latest version of CubeMx and use the board selector:
2026-02-27 3:21 AM
@Andrew Neil wrote:
I don't see the PLAY mentioned on the STM32H5E4/5F4 or STM32H5E5/5F5 pages ?
Will be escalated.
2026-02-27 3:28 AM
@mƎALLEm wrote:There will be a Discovery and a NUCLEO boards ;).. Stay tuned.
And an App Note ... ?
2026-02-27 3:35 AM
@Andrew Neil wrote:
@mƎALLEm wrote:
There will be a Discovery and a NUCLEO boards ;).. Stay tuned.
And an App Note ... ?
Of course like usual for any new STM32 series.. and a dedicated application note will be also available for PLAY.
2026-02-27 4:11 AM - edited 2026-02-27 4:16 AM
Is there a simulator for this? I'd love to play with it without hardware.
I'd love to try to generate custom waveforms, hardware acceleration for certain operators, custom communication peripherals, etc.
2026-02-27 4:36 AM
It seems fairly simple - not sure it would warrant a simulator ... ?
2026-02-27 4:40 AM
@unsigned_char_array wrote:
Is there a simulator for this? I'd love to play with it without hardware.
I'd love to try to generate custom waveforms, hardware acceleration for certain operators, custom communication peripherals, etc.
That's not a true FPGA, CPLD or similar device. It's just a lookup table that you could construct some logic block with.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.