2023-11-09 10:02 PM
I use J-Link and STM32G474, which can burn the program, but can't erase the chip. After trying to use J-Link STM to unlock the chip, it also did not work
Application log started
- J-Flash V7.92b (J-Flash compiled Aug 23 2023 14:00:43)
- JLinkARM.dll V7.92b (DLL compiled Aug 23 2023 14:00:04)
Reading flash device list [C:\Program Files\SEGGER\JLink\ETC/JFlash/Flash.csv] ...
- List of flash devices read successfully (451 Devices)
Reading MCU device list ...
- List of MCU devices read successfully (10201 Devices)
Opening project file [C:\Users\PC\AppData\Roaming\SEGGER\Default.jflash] ...
- Project opened successfully
Opening data file [E:\JOJOTester_HM\Testinfo\291\data\STM32G4xx-Kernel.bin] ...
- Data file opened successfully (5368 bytes, 1 range, CRC of data = 0x86DE39CB, CRC of file = 0x86DE39CB)
Opening data file [E:\JOJOTester_HM\Testinfo\291\data\STM32G4xx-Kernel.bin] ...
- Data file opened successfully (5368 bytes, 1 range, CRC of data = 0x86DE39CB, CRC of file = 0x86DE39CB)
Connecting ...
- Connecting via USB to probe/ programmer device 0
- Probe/ Programmer firmware: J-Link V12 compiled Aug 2 2023 10:34:27
- Probe/ Programmer S/N: 602004233
- Device "STM32G474VE" selected.
- Target interface speed: 4000 kHz (Fixed)
- VTarget = 3.309V
- InitTarget() start
- JTAG selected. Identifying JTAG Chain...
- TotalIRLen = 9, IRPrint = 0x0011
- JTAG chain detection found 2 devices:
- #0 Id: 0x4BA00477, IRLen: 04, CoreSight JTAG-DP
- #1 Id: 0x16469041, IRLen: 05, Unknown device
- JTAG Chain Identified. Connecting to DAP TAP...
- Successfully connected to selected DAP TAP.
- DAP initialized successfully.
- InitTarget() end - Took 12.1ms
- TotalIRLen = 9, IRPrint = 0x0011
- JTAG chain detection found 2 devices:
- #0 Id: 0x4BA00477, IRLen: 04, CoreSight JTAG-DP
- #1 Id: 0x16469041, IRLen: 05, Unknown device
- DPv0 detected
- Scanning AP map to find all available APs
- AP[1]: Stopped AP scan as end of AP map has been reached
- AP[0]: AHB-AP (IDR: 0x24770011)
- Iterating through AP map to find AHB-AP to use
- AP[0]: Core found
- AP[0]: AHB-AP ROM base: 0xE00FF000
- CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
- Found Cortex-M4 r0p1, Little endian.
- FPUnit: 6 code (BP) slots and 2 literal slots
- CoreSight components:
- ROMTbl[0] @ E00FF000
- [0][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7
- [0][1]: E0001000 CID B105E00D PID 003BB002 DWT
- [0][2]: E0002000 CID B105E00D PID 002BB003 FPB
- [0][3]: E0000000 CID B105E00D PID 003BB001 ITM
- [0][4]: E0040000 CID B105900D PID 000BB9A1 TPIU
- [0][5]: E0041000 CID B105900D PID 000BB925 ETM
- Executing init sequence ...
- Initialized successfully
- Target interface speed: 4000 kHz (Fixed)
- Found 2 JTAG devices. Core ID: 0x4BA00477 (None)
- Connected successfully
Auto programming target (5368 bytes, 1 range) ...
- Checking if selected data fits into selected flash sectors.
- Start of determining flash info (Bank 0 @ 0x08000000)
- End of determining flash info
- Flash bank info:
- 128 * 2 KB @ 0x08000000
- 128 * 2 KB @ 0x08040000
- Start of preparing flash programming
- End of preparing flash programming
- Start of determining dirty areas in flash cache
- End of determining dirty areas
- CPU is running at 56000 kHz.
- Start of erasing sectors
- Blank checking 0x08000000 - 0x080017FF
- Erasing range 0x08000000 - 0x080017FF ( 3 Sectors, 6 KB)
- End of erasing sectors
- Start of flash programming
- Programming range 0x08000000 - 0x080017FF ( 3 Sectors, 6 KB)
- End of flash programming
- Flash programming performed for 1 range (6144 bytes)
- 0x8000000 - 0x80017FF ( 3 Sectors, 6 KB)
- Start of verifying flash
- End of verifying flash
- Start of restoring
- End of restoring
- Executing exit sequence ...
- De-initialized successfully
- Target erased, programmed and verified successfully - Completed after 0.189 sec
Opening data file [E:\JOJOTester_HM\Testinfo\291\data\p291-Headcontroller-Bootloader.bin] ...
- Data file opened successfully (42160 bytes, 1 range, CRC of data = 0xEEF31461, CRC of file = 0xEEF31461)
Auto programming target (42160 bytes, 1 range) ...
- Checking if selected data fits into selected flash sectors.
- Start of determining flash info (Bank 0 @ 0x08000000)
- End of determining flash info
- Flash bank info:
- 128 * 2 KB @ 0x08000000
- 128 * 2 KB @ 0x08040000
- Start of preparing flash programming
- End of preparing flash programming
- Start of determining dirty areas in flash cache
- End of determining dirty areas
- CPU speed could not be measured.
- Start of erasing sectors
- Blank checking 0x08005000 - 0x0800F7FF
- Erasing range 0x08005000 - 0x0800F7FF ( 21 Sectors, 42 KB)
- End of erasing sectors
- Start of flash programming
- Programming range 0x08005000 - 0x0800CFFF ( 16 Sectors, 32 KB)
- Programming range 0x0800D000 - 0x0800F7FF ( 5 Sectors, 10 KB)
- End of flash programming
- Flash programming performed for 1 range (43008 bytes)
- 0x8005000 - 0x800F7FF ( 21 Sectors, 42 KB)
- Start of verifying flash
- End of verifying flash
- Start of restoring
- End of restoring
- Executing exit sequence ...
- De-initialized successfully
- Target erased, programmed and verified successfully - Completed after 1.092 sec
Opening data file [E:\JOJOTester_HM\Testinfo\291\data\P291-HeadControl-FactoryApp.bin] ...
- Data file opened successfully (154141 bytes, 1 range, CRC of data = 0x563A56AF, CRC of file = 0x563A56AF)
Auto programming target (154141 bytes, 1 range) ...
- Checking if selected data fits into selected flash sectors.
- Start of determining flash info (Bank 0 @ 0x08000000)
- End of determining flash info
- Flash bank info:
- 128 * 2 KB @ 0x08000000
- 128 * 2 KB @ 0x08040000
- Start of preparing flash programming
- End of preparing flash programming
- Start of determining dirty areas in flash cache
- End of determining dirty areas
- CPU speed could not be measured.
- Start of erasing sectors
- Blank checking 0x08020000 - 0x0803FFFF
- Erasing range 0x08020000 - 0x0803FFFF ( 64 Sectors, 128 KB)
- Blank checking 0x08040000 - 0x08045FFF
- Erasing range 0x08040000 - 0x08045FFF ( 12 Sectors, 24 KB)
- End of erasing sectors
- Start of flash programming
- Programming range 0x08020000 - 0x08027FFF ( 16 Sectors, 32 KB)
- Programming range 0x08028000 - 0x0802FFFF ( 16 Sectors, 32 KB)
- Programming range 0x08030000 - 0x08037FFF ( 16 Sectors, 32 KB)
- Programming range 0x08038000 - 0x0803FFFF ( 16 Sectors, 32 KB)
- Programming range 0x08040000 - 0x08045FFF ( 12 Sectors, 24 KB)
- End of flash programming
- Flash programming performed for 1 range (155648 bytes)
- 0x8020000 - 0x8045FFF ( 76 Sectors, 152 KB)
- Start of verifying flash
- End of verifying flash
- Start of restoring
- End of restoring
- Executing exit sequence ...
- De-initialized successfully
- Target erased, programmed and verified successfully - Completed after 3.817 sec
Erasing chip ...
- 258 sectors, 3 ranges, 0x8000000 - 0x807FFFF, 0x1FFF7800 - 0x1FFF782F, 0x1FFFF800 - 0x1FFFF82F
- Start of determining flash info (Bank 0 @ 0x08000000)
- End of determining flash info
- Flash bank info:
- 128 * 2 KB @ 0x08000000
- 128 * 2 KB @ 0x08040000
- Start of preparing flash programming
- End of preparing flash programming
- Start of determining dirty areas in flash cache
- End of determining dirty areas
- CPU speed could not be measured.
- Start of erasing chip
- ERROR: Failed to erase chip.
Failed to execute RAMCode for chip erase!
- End of erasing chip
- ERROR: Erase failed
- Start of restoring
- End of restoring
- ERROR: Failed to erase chip
Disconnecting ...
- OnDisconnectTarget() start
- OnDisconnectTarget() end - Took 10us
- Disconnected
2023-11-13 5:38 AM
Hello @kerry1
If you are using a customized board, it is very likely that the issue is linked to fluctuating/insufficient power or loose connection. If you have nucleo or disco board you can upgrade the ST Link with specific version of J Link firmware.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.