2025-05-22 7:15 PM
Hi ST teams,
I use STM32G473VET3 on my design. On the datasheet, SPI4 had 3 NSS pins hardware: PE3, PE4 and PE11.
If I use other GPIO excluding for the NSS pin function, there are any potential issue?
Ex: SPI bus can not work at maximum speed.
On my design, I use SPI4 is master and PF2, PF9, PE3, PE4, PE5 for slave chip select function.
Thanks.
2025-05-22 7:22 PM
If you're controlling the CS/NSS pins manually (GPIO output and toggle), there are no downsides to choosing a different pin. It won't affect max clock rate.
If you have multiple slaves, you have no choice but to control CS/NSS manually.
2025-05-22 7:33 PM
Thank you for reply.
So i understand that there are no issue/limited when control CS/NSS manually instead use "automatic" CS/NSS control?
2025-05-26 5:37 PM
Yes
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.