2018-08-09 7:10 AM
Today I bought an evaluation board. After starting it display the current demo. If I select TouchGFX or Embedded Wizard demo these applications are displaying wrong. The screen is splitten in two halfs. Each one ist refreshing differently. Then the display is distorsioned.
Is this normal?, Is this a problem of these demo applications or the board has a defect?
2018-08-09 8:24 AM
Hello,
Which revision of the board are you using?
Which firmware package version are you using to build the demo?
With Regards,
Imen.
2018-08-09 9:46 PM
Hello,
Thanks.
The Revision of the board is B-02. The firmware is V2.J31.M21.
The Demo application is 1.0.0. I do no build the application. This is the original one.
I tried now the binary (full demo) included with STM32Cube_FW_F7_V1.12.0 too (Projects\STM32F769I_EVAL\Demonstration\STemWin\Binary). This does not change the wrong behavior.
Regards.
2018-08-23 12:53 AM
Hello,
I returned the board and now I have a new one, STM32F769 -EVAL. With the new board is working fine now. The new board has not the problem with the TouchGFX and Embedded Wizard DEmos in the Board demonstration application.
But the version of the demonstration application is now 1.2.0. The binary Demonstration application in the Firmware STM32Cube_FW_F7_V1.12.0 has the version 1.0.0. Where can I download the new binary (1.2.0)?. The current firmware STM32Cube_FW_F7_V1.12.0 contents an old version.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.