2024-05-30 12:29 AM - edited 2024-06-03 7:26 AM
I am building a circuit board using STM32F765. After building it I can use stlink to burn the firmware (stm32 utility) via SWD and read the chip correctly, but I can't get into the bootloader and I can't use the serial port (USB) to read the chip on my PC.
Make sure the power supply is normal. I'm not sure what's going on here.
2024-06-25 10:28 AM
Dear @yushangchen ,
Can you give more details with a log when booting from Internal bootloader with BOOT0 pins ? and use the STM32CubeProgrammer either via UART or USB ( DFU).
Some hints :
0) Picture of the top marking and revision
1) Let us know the schematics and especially the used crystal HSE XXMHz.
2) try to measure the HSI - Internal 16MHz RC used in the internal booloader and output via a code in flash on MCO - PA8 pin.
Hope it helps.
STOne-32.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.