2018-05-16 7:13 AM
Hi, i have big issues with a STM32F746 + RTOS + LWIP. Initialcode is generated by CubeMX.
The Problem: I ping with the device and every second paket get responded with a delay of 800-1000 ms or dropped/timeouted. There a 2 UDP-Services that accept pakets on two dedicated Ports,
they also have the same problem. If i increase the rate of UDP-Requests, the ICMP/UDP respond time is a very low ( a 1 ms ).I think some periodic Task from the LWIP get not often enough called.
Had anyone an idea where to look ?
Best regards and Thanks,
NiklasWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.