2017-07-18 7:21 AM
Hi, I'm working with STM32F745VE
I have problem with ADC trigger and UART DMA normal mode.1. I try trigger adc1 by timer2 update event, but it work only with
timer8 update
2. static void UART_DMATransmitCplt(DMA_HandleTypeDef *hdma) doesn't call HAL_UART_TxCpltCallback(huart) in
/* DMA Normal mode*/
if((hdma->Instance->CR & DMA_SxCR_CIRC) == 0U){
}
Solved! Go to Solution.
2017-11-08 8:52 AM
STM32F74xxx STM32F75xxx Errata sheet
Workarounds• For TIM1 and TIM8 TRGO or TRGO 2 events: select the trigger detection on both the rising and falling edges. The EXTEN[1:0] or JEXTEN[1:0] bits must be set to 0x11 in the ADC_CR2 register.
• For TIM2/TIM4/TIM5/TIM6/ TRGO or TGRO2 events: enable the DAC peripheral clock in the RCC_APB1ENR register
2017-11-08 8:52 AM
STM32F74xxx STM32F75xxx Errata sheet
Workarounds• For TIM1 and TIM8 TRGO or TRGO 2 events: select the trigger detection on both the rising and falling edges. The EXTEN[1:0] or JEXTEN[1:0] bits must be set to 0x11 in the ADC_CR2 register.
• For TIM2/TIM4/TIM5/TIM6/ TRGO or TGRO2 events: enable the DAC peripheral clock in the RCC_APB1ENR register
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.