2017-06-20 6:29 AM
Hello all,
Does anyone has a USART Rx working with DMA + FIFO in circular mode?
#dma #stm32f7 #fifo #circular-mode2017-06-20 8:38 AM
I don't see bandwidth being an issue needing to use FIFO mode DMA, it's not an SDIO or DCMI interface delivering >10MBps
2017-06-20 12:31 PM
Hello Clive,
It is not, but as i am learning the F7 i would like to try it.
On the DMA topic...if i remember correctly (i hope my memory is good ) , on the old forum, you had a post for F4 stating that you can trigger a transfer when a
match char
is detected? I intend to use the DMA for an Xbee communication.if true, do you still have the link? i tied to find it but i cant or...i'm dreaming
2017-06-20 4:45 PM
The FIFO options represent a handful of additional settings, if you can set up the Circular DMA you'd be 95% the way there.
I don't recall a pattern match method for the USART, you could trigger via a TIM on a periodic basis.
The were some TIM+DMA+GPIO examples outputting pattern-buffers
2017-07-03 10:01 AM
Hi,
In RM0385 i have found that a character match can be used by using CMF/CMIE + ADD[0:7] from USART_ISR/USART_CR1 + USART CR2. I will try to see if i can make it work
2017-07-03 10:11 AM
DMA + FIFO stores / reads the main memory in blocks of 4 bytes or 8 bytes. But the USART can stop reading in one byte. In this case, the data will be lost.
Additionally, in ring mode (DMA_SxNDTR) = 0xFFFF, constantly !!!2017-07-03 5:08 PM
Hello Clive,
I made a try for char match '$' and is working with the following setup
volatile uint32_t myUART_ISR_Val;
void MX_UART7_Init(void)
{ huart7.Instance = UART7; huart7.Init.BaudRate = 115200; huart7.Init.WordLength = UART_WORDLENGTH_8B; huart7.Init.StopBits = UART_STOPBITS_1; huart7.Init.Parity = UART_PARITY_NONE; huart7.Init.Mode = UART_MODE_TX_RX; huart7.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart7.Init.OverSampling = UART_OVERSAMPLING_16; huart7.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart7.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;if (HAL_UART_Init(&huart7) != HAL_OK)
{ _Error_Handler(__FILE__, __LINE__); } //Character match interrupt enable //A USART interrupt is generated when the CMF bit is set in the USART_ISR register SET_BIT(huart7.Instance->CR1, USART_CR1_CMIE); /* Disable the Peripheral */ __HAL_UART_DISABLE(&huart7); //$ is 36 in DEC MODIFY_REG(huart7.Instance->CR2, USART_CR2_ADD, ((uint32_t)36 << UART_CR2_ADDRESS_LSB_POS)); /* Enable the Peripheral */ __HAL_UART_ENABLE(&huart7); }void UART7_IRQHandler(void)
{
myUART_ISR_Val = READ_REG(huart7.Instance->ISR);
//clear USART_ICR_CMCF
huart7.Instance->ICR |= 1 << 17;
HAL_UART_IRQHandler(&huart7);
}
and in main i do the check
MX_GPIO_Init();
MX_DMA_Init(); MX_UART7_Init(); MX_ADC1_Init();Xbee_Init();//RX DMA circular - TX DMA normal
_isrflags = READ_REG(huart7.Instance->ISR); _icrflags = READ_REG(huart7.Instance->ICR); _cr1its = READ_REG(huart7.Instance->CR1); _cr2its = READ_REG(huart7.Instance->CR2); _cr3its = READ_REG(huart7.Instance->CR3); printf('_isrflags = %d\r\n', _isrflags); printf('_icrflags = %d\r\n', _icrflags); printf('_cr1its = %d\r\n', _cr1its); printf('_cr2its = %d\r\n', _cr2its); printf('_cr3its = %d\r\n', _cr3its); printf('Init is done\r\n');while (1) {if(myUART_ISR_Val){ printf('myUART_ISR_Val = %d\r\n', myUART_ISR_Val); myUART_ISR_Val = 0; }}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.