2015-08-04 1:58 PM
The STM32F7 HAL Driver (v1.1.0) has a bug in the __HAL_UART_CLEAR_IT macro:
Writing a bit to the ICR register clears the corresponding interrupt; however the __HAL_UART_CLEAR_IT writes the ones-complement:&sharpdefine __HAL_UART_CLEAR_IT(__HANDLE__, __FLAG__) ((__HANDLE__)->Instance->ICR = ~(__FLAG__))The corresponding USART macro is implemented correctly:&sharpdefine __HAL_USART_CLEAR_IT(__HANDLE__, __IT_CLEAR__) ((__HANDLE__)->Instance->ICR = (uint32_t)(__IT_CLEAR__))- Malcolm #stm32f7-hal-uart2015-08-04 4:59 PM
The [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx]STM32 Software Tools and Firmware forum page might be a better venue for these bugs.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.