2016-09-06 2:59 AM
Hello All,
If I am using one of the NAND FLASHes from Spansion (Cypress) such as the S34ML08G2 - is BCH ECC supported in hardware?Thanks,John W. #stm43f7-fmc2016-09-06 6:21 AM
RM0385 13.6.6:
The ECC algorithm implemented in the FMC can perform 1-bit error correction and 2-biterror detection per 256, 512, 1 024, 2 048, 4 096 or 8 192 bytes read or written from/to the
NAND Flash memory. It is based on the Hamming coding algorithm and consists in
calculating the row and column parity.
JW
2016-09-06 8:03 AM
Generally there has been a movement to letting the NAND chips compute and check syndrome data as the bit level and array structures have become more exotic/complex. The chip vendor should be able to supply host level ''correction'' software/drivers that can resolve error flagged in the checking process.
2016-09-08 3:24 AM
Does ST have a list of compatible NAND FLASH memories for their microcontrollers?
Thanks.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.