2017-10-19 1:37 PM
Hello,
I'm new to STM32F7 and not familiar with the design environment. I'm setting up 2 UART channels and in CubeMX I setup each UART channel to use normal DMA buffer instead of circular. Here is a sample of what I'm trying to do.
HAL_UART_Init(&huart1);
HAL_UART_Init(&huart6);uint8_t buffer1a[] = {0xFF, 0xD7};
uint8_t buffer1b[] = {0xFF, 0xCF, 0x00, 0x00, 0x00, 0x0A, 0x00, 0x32, 0x00, 0x46, 0xF8, 0x00};HAL_UART_Transmit_DMA(&huart1, buffer1a, sizeof(buffer1a));
HAL_UART_Transmit_DMA(&huart6, buffer1a, sizeof(buffer1a)); HAL_Delay(500);while (1)
{HAL_UART_Transmit_DMA(&huart1, buffer1b, sizeof(buffer1b)); HAL_UART_Transmit_DMA(&huart6, buffer1b, sizeof(buffer1b));HAL_Delay(1000);
}
I need to change buffer1b in the while(1) loop and send out new data.
The first 2 DMA transfers work fine but the DMA transfers in the while(1) loop does not work at all.
What do I need to get this working.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.