2012-11-02 12:09 AM
In STM32F4xx.H the bits DBGMCU_APB2... are erroneously named DBGMCU_APB1... - just info.
2012-11-02 3:02 AM
These ones
/******************** Bit definition for DBGMCU_APB2_FZ register ************/
#define DBGMCU_APB1_FZ_DBG_TIM1_STOP ((uint32_t)0x00000001)
#define DBGMCU_APB1_FZ_DBG_TIM8_STOP ((uint32_t)0x00000002)
#define DBGMCU_APB1_FZ_DBG_TIM9_STOP ((uint32_t)0x00010000)
#define DBGMCU_APB1_FZ_DBG_TIM10_STOP ((uint32_t)0x00020000)
#define DBGMCU_APB1_FZ_DBG_TIM11_STOP ((uint32_t)0x00040000)
Thanks for the FYI
2013-01-03 2:42 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.